How Do I Activate Version 2.7 of CodeWarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How Do I Activate Version 2.7 of CodeWarrior

跳至解决方案
2,316 次查看
usr4691
Contributor I

I have a license for CodeWarrior 2.9. I also want to activate v2.7 because the development team that I am working with also uses v2.7 to develop their code.

标签 (1)
0 项奖励
回复
1 解答
2,185 次查看
stanish
NXP Employee
NXP Employee

Hello Braton,


according to the screenshot you sent it seems this is not a licensing issue.

This is probably a linker issue/defect.

Anyway I've posted a temporary CW for MPC55xx/56xx v2.x license.dat which should work with v2.7.

Please check again with the license attached. (the license will expire 10-nov-2013)

This might be related to a linker defect which was fixed in a newer release.


Is someone else from your team able to build the project using same CW version (v2.7)?


Stan

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,185 次查看
TICS_Fiona
NXP Employee
NXP Employee

Could you please contact license team (license@freescale.com) to get the license for CW2.7?  Please also attach your license file for CW2.9, which contains the info of your license type, and locked ID. Thanks!

0 项奖励
回复
2,185 次查看
usr4691
Contributor I

I copied the license.dat to my CodeWarrior v2.7 directory but it did not work.

0 项奖励
回复
2,185 次查看
stanish
NXP Employee
NXP Employee

Hello Braton,

What do you observe on your side? can you send a screenshot of a licensing error you get?

Do you have both versions installed on the same PC? if not then make sure the license.dat you use may be locked to a particular machine so it may not work on any other machine.

Stan

0 项奖励
回复
2,185 次查看
usr4691
Contributor I

This is what I get when I attempt to build my firmware using CodeWarrior v2.7


ELFError.jpg

0 项奖励
回复
2,186 次查看
stanish
NXP Employee
NXP Employee

Hello Braton,


according to the screenshot you sent it seems this is not a licensing issue.

This is probably a linker issue/defect.

Anyway I've posted a temporary CW for MPC55xx/56xx v2.x license.dat which should work with v2.7.

Please check again with the license attached. (the license will expire 10-nov-2013)

This might be related to a linker defect which was fixed in a newer release.


Is someone else from your team able to build the project using same CW version (v2.7)?


Stan

0 项奖励
回复
2,185 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

from the license policy that, only the latest CW version can be actived.

but mostly, Freescal license is backward compatiable. 2.9 license could also work for 2.7. please try it.

0 项奖励
回复