Hello. MPC5674F Link Command File (LCF) is being created. I want to enter unique information in the LCF. Is there a way to declare a symbol for unique information in the MPC5674F LCF and enter its symbol value?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hello. MPC5674F Link Command File (LCF) is being created. I want to enter unique information in the LCF. Is there a way to declare a symbol for unique information in the MPC5674F LCF and enter its symbol value?

1,697 次查看
choonharyu
Contributor I

MEMORY
{
    /* FLASH: 0x00000000 - 0x0003FFFFF */
    /* Fixed location required for RCHW and program entry point*/
    resetvector:           org = 0x00000000,   len = 0x00000008

    /* Contains initializations from __ppc_eabi_init.c,
     MPC56xx_HWInit.c, MPC56xx_init_*.c and the entry point (__startup).
     Should be 4K since the hardware automatically creates a default TLB entry
     from the start of the entry point specified in RCHW.
     */
    init:                   org = 0x00000010,   len = 0x00000FF0 /* ~4K */

    /* ~63K gap required to align the exception handlers.*/

    /* Contains interrupt branch tables for both core and INTC module
     and the ISR handlers code. Note, the gap is required since the vector
     base address field of core IVPR is defined within the range [0:15], the
     INTC branch tables must be loaded at an address aligned to 64K boundary.
     */
    exception_handlers: org = 0x00010000,   len = 0x0020000 /* 128K */

    /* Space allocated for user code and device initialization.
    ROM Image address should be set with the start address of this
    segment in order to instruct the runtime to initialize the
    static variables. All the section above are ignored for this action.
    Please see -romaddr linker option.*/
    internal_flash:        org = 0x00030000,   len = 0x003D0000 /* 3904K */

    /* SRAM: 0x40000000 - 0x4003FFFF */
    internal_ram:       org = 0x40000000,   len = 0x00030000 /* 192KB */
    heap  :             org = 0x40030000,   len = 0x00008000 /* 32KB Heap start location */
    stack :             org = 0x40038000,   len = 0x00008000 /* 32KB Start location for Stack */
 


    /* ROM SW ID */
    rom_sw_id:    org = 0x40035000,   len = 0x0000000D
}

SECTIONS
{

 GROUP : {
   /* I want to fill the value of symbol */
 } > rom_sw_id

}

0 项奖励
回复
1 回复

1,485 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I would suggest you submit a private case for this question.

https://community.nxp.com/docs/DOC-329745 

Please detail what result you expect.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复