HC12: FLASH/EEPROM write

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HC12: FLASH/EEPROM write

ソリューションへジャンプ
3,634件の閲覧回数
EM1
Contributor I
Hello,
can anybody please help me in this issue.
I have a HCS12 (MC9S12DP512), and I want to use the flash and the eeprom for data logging.
so I want to place variables in flash memory (banked), and in the eeprom.
I didn't find any code (or libraries) to write to FLASH in the codewarrior.
 
does anybody have an idea how to place variables in flash and how to write to it?
 
thanks a lot.
 
EM1.

Message Edited by CrasyCat on 2007-04-13 11:31 AM

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,174件の閲覧回数
Alban
Senior Contributor II
Hello and Welcome EM1.
 
Product specific questions should be asked in the product board.
Only CodeWarrior related questions are to be posted in CodeWarrior board.
 
The use of the search engine functionality (see at bottom of page) would have allowed you to discover elements for your answer: Flash/EEPROM on 16-Bit board.
 
Cheers,
Alban.
 
 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,175件の閲覧回数
Alban
Senior Contributor II
Hello and Welcome EM1.
 
Product specific questions should be asked in the product board.
Only CodeWarrior related questions are to be posted in CodeWarrior board.
 
The use of the search engine functionality (see at bottom of page) would have allowed you to discover elements for your answer: Flash/EEPROM on 16-Bit board.
 
Cheers,
Alban.
 
 
0 件の賞賛
返信