HC12: FLASH/EEPROM write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HC12: FLASH/EEPROM write

Jump to solution
3,622 Views
EM1
Contributor I
Hello,
can anybody please help me in this issue.
I have a HCS12 (MC9S12DP512), and I want to use the flash and the eeprom for data logging.
so I want to place variables in flash memory (banked), and in the eeprom.
I didn't find any code (or libraries) to write to FLASH in the codewarrior.
 
does anybody have an idea how to place variables in flash and how to write to it?
 
thanks a lot.
 
EM1.

Message Edited by CrasyCat on 2007-04-13 11:31 AM

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,162 Views
Alban
Senior Contributor II
Hello and Welcome EM1.
 
Product specific questions should be asked in the product board.
Only CodeWarrior related questions are to be posted in CodeWarrior board.
 
The use of the search engine functionality (see at bottom of page) would have allowed you to discover elements for your answer: Flash/EEPROM on 16-Bit board.
 
Cheers,
Alban.
 
 

View solution in original post

0 Kudos
Reply
1 Reply
2,163 Views
Alban
Senior Contributor II
Hello and Welcome EM1.
 
Product specific questions should be asked in the product board.
Only CodeWarrior related questions are to be posted in CodeWarrior board.
 
The use of the search engine functionality (see at bottom of page) would have allowed you to discover elements for your answer: Flash/EEPROM on 16-Bit board.
 
Cheers,
Alban.
 
 
0 Kudos
Reply