Fill unused flash memory on MPC5604B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fill unused flash memory on MPC5604B

ソリューションへジャンプ
3,253件の閲覧回数
jean-christoph7
Contributor III

Hello,

 

I'm using Codewarrior 10.6 for MCU, and I want to know if it is possible to force codewarrior to fill the unused flash memory with a defined value, because actually the unused flash memory is fill with 0xFF and I need to change it.

 

Have you an example?

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,999件の閲覧回数
jean-christoph7
Contributor III

Perfect.

Thanks a lot.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,998件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

look at the app note in the attachment. In section 5, there is the description, how to fill unused flash memory with predefined pattern.

Regards,

Martin

0 件の賞賛
返信
3,000件の閲覧回数
jean-christoph7
Contributor III

Perfect.

Thanks a lot.

0 件の賞賛
返信