Fill unused flash memory on MPC5604B

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Fill unused flash memory on MPC5604B

跳至解决方案
3,248 次查看
jean-christoph7
Contributor III

Hello,

 

I'm using Codewarrior 10.6 for MCU, and I want to know if it is possible to force codewarrior to fill the unused flash memory with a defined value, because actually the unused flash memory is fill with 0xFF and I need to change it.

 

Have you an example?

 

Thanks.

标签 (1)
0 项奖励
回复
1 解答
2,994 次查看
jean-christoph7
Contributor III

Perfect.

Thanks a lot.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,993 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

look at the app note in the attachment. In section 5, there is the description, how to fill unused flash memory with predefined pattern.

Regards,

Martin

0 项奖励
回复
2,995 次查看
jean-christoph7
Contributor III

Perfect.

Thanks a lot.

0 项奖励
回复