Fill unused flash memory on MPC5604B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fill unused flash memory on MPC5604B

Jump to solution
3,225 Views
jean-christoph7
Contributor III

Hello,

 

I'm using Codewarrior 10.6 for MCU, and I want to know if it is possible to force codewarrior to fill the unused flash memory with a defined value, because actually the unused flash memory is fill with 0xFF and I need to change it.

 

Have you an example?

 

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
2,971 Views
jean-christoph7
Contributor III

Perfect.

Thanks a lot.

View solution in original post

0 Kudos
Reply
2 Replies
2,970 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

look at the app note in the attachment. In section 5, there is the description, how to fill unused flash memory with predefined pattern.

Regards,

Martin

0 Kudos
Reply
2,972 Views
jean-christoph7
Contributor III

Perfect.

Thanks a lot.

0 Kudos
Reply