Error import project in CW10.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error import project in CW10.4

跳至解决方案
2,554 次查看
kappa74
Contributor IV

Good morning,

I'm passing from CW10.2 to CW10.4.

I installed CW10.4 but and then I imported the project in the nwe workspace.

When I import the project I get always the error:

"An internal error has occurred.

String index out of range: -1"

5750_5750.pngpastedImage_0.png

 

Which string is in error?

Why do I get it?

Thank you

Best Regards

Mirko

标签 (1)
0 项奖励
回复
1 解答
2,386 次查看
kappa74
Contributor IV

I attached the 2 files project

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,386 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

can you upload your project for us to check?

0 项奖励
回复
2,387 次查看
kappa74
Contributor IV

I attached the 2 files project

0 项奖励
回复