Error import project in CW10.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error import project in CW10.4

ソリューションへジャンプ
3,488件の閲覧回数
kappa74
Contributor IV

Good morning,

I'm passing from CW10.2 to CW10.4.

I installed CW10.4 but and then I imported the project in the nwe workspace.

When I import the project I get always the error:

"An internal error has occurred.

String index out of range: -1"

5750_5750.pngpastedImage_0.png

 

Which string is in error?

Why do I get it?

Thank you

Best Regards

Mirko

ラベル(1)
0 件の賞賛
返信
1 解決策
3,320件の閲覧回数
kappa74
Contributor IV

I attached the 2 files project

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,320件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

can you upload your project for us to check?

0 件の賞賛
返信
3,321件の閲覧回数
kappa74
Contributor IV

I attached the 2 files project

0 件の賞賛
返信