Error can not open ansiis.lib file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error can not open ansiis.lib file

Jump to solution
2,342 Views
Sunil_Reddy
Contributor I

Hi all

I am using Code Warrior on Windows 7 platform. When I do Build Project (Build All) I am getting an error message as below 


"can not open file "C:\.......\ansiis.lib"

ELF: can not open file "C:\.......\ansiis.lib"

Had anyone encountered similar kind of problem? What could be the reason of this problem? How to add/delete the ansiis.lib files? 

 

Thank you very much 

 

Sunil 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,823 Views
kef
Specialist I

Are you porting S08 project to S12?

CW for S12 doesn't have ansiis.lib, but it has ansisi.lib.

CW for S08 doesn't have ansisi.lib, but it has ansiis.lib.

View solution in original post

0 Kudos
Reply
1 Reply
1,824 Views
kef
Specialist I

Are you porting S08 project to S12?

CW for S12 doesn't have ansiis.lib, but it has ansisi.lib.

CW for S08 doesn't have ansisi.lib, but it has ansiis.lib.

0 Kudos
Reply