Error can not open ansiis.lib file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error can not open ansiis.lib file

ソリューションへジャンプ
2,344件の閲覧回数
Sunil_Reddy
Contributor I

Hi all

I am using Code Warrior on Windows 7 platform. When I do Build Project (Build All) I am getting an error message as below 


"can not open file "C:\.......\ansiis.lib"

ELF: can not open file "C:\.......\ansiis.lib"

Had anyone encountered similar kind of problem? What could be the reason of this problem? How to add/delete the ansiis.lib files? 

 

Thank you very much 

 

Sunil 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,825件の閲覧回数
kef
Specialist I

Are you porting S08 project to S12?

CW for S12 doesn't have ansiis.lib, but it has ansisi.lib.

CW for S08 doesn't have ansisi.lib, but it has ansiis.lib.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,826件の閲覧回数
kef
Specialist I

Are you porting S08 project to S12?

CW for S12 doesn't have ansiis.lib, but it has ansisi.lib.

CW for S08 doesn't have ansisi.lib, but it has ansiis.lib.

0 件の賞賛
返信