Does WCT1012 15W Single coil Tx V3.1 work with Codewarrior V11.1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does WCT1012 15W Single coil Tx V3.1 work with Codewarrior V11.1?

1,857件の閲覧回数
kim1
Contributor I

Hi!

Using the NXP wireless charger with software is not really straightforward. I am very having trouble with this issue. Whenever I try to follow the manual with the recent CodeWarrior V11.1: https://www.nxp.com/docs/en/user-guide/WCT1012V31SYSUG.pdf which is based on V10.7 CodeWarrior, it doesn't work at all from page 18. This is about installing MCU v10.7 service package. But this package requires V10.7 CodeWarrior which is not provided. I also tried the previous solutions, but none of them is working for now.

https://community.nxp.com/t5/CodeWarrior-Development-Tools/WCT-15W1CFFPD-Codewarrior-v11-1-software-...

https://community.nxp.com/t5/CodeWarrior-Development-Tools/Cannot-complete-the-install-Service-Pack-...

Also, downloading the previous V10.7 is not supported for now.

https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-Download-Previous-Version-CodeWarr...

At this moment, I am really confused about that WCT1012 15W Single coil Tx V3.1 is really supported by CodeWarrior and other software in the product manual. CodeWarrior V11.1 does not support the device, and I even don't know whether CodeWarrior V10.7 would work or not because I don't have it.

If this wireless charger is not supposed to work with any software here, can you recommend any 15W  single coil device that I really am able to control the charger with software?

0 件の賞賛
返信
5 返答(返信)

1,835件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think that the CW for mcu ver11.x supports MWCT1012.

If you import the MWCT1012 project to CW for mcu ver11.x, can you compile and link successfully?

BR

XiangJun Rong

0 件の賞賛
返信

1,825件の閲覧回数
kim1
Contributor I

Thank you for your help, Xiangjun_rong.

Yes, I guess CW v11.1 works with WCT1012 15W single coil Tx v3.1. But, the libraries regarding wireless charging on the manual cannot be installed because:

1. the service pack which is required from the manual is version 10.7 which is not compatible with CW v11.1. Also library link for the device does not work at all. https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=WCT1012_15W1COIL_V3.1&appType=moder...

2. CW 10.7 is not provided when I try to follow this link:https://community.nxp.com/t5/CodeWarrior-Development-Tools/How-to-Download-Previous-Version-CodeWarr...

This shows lock icon..

kim1_0-1628539925518.png

 

 

I am struggling with this because even simply following the manual does not guarantee the expected results on the manual...

0 件の賞賛
返信

1,819件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kim,

If you do not install any patch, just import the project of WCT1012 15W Single coil Tx V3.1 project to CodeWarrior for mcu ver11.x, can you compile and debug?

BR

XiangJun Rong

0 件の賞賛
返信

1,814件の閲覧回数
kim1
Contributor I

Thank you for your reply, Xiangjun_rong

The thing is I cannot download "WCT1012 15W Single coil Tx V3.1" file on the previously attached image. You can try to download it. It always shows a blank page whenever I try to download it.

0 件の賞賛
返信

1,807件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

NXP policy has changed, the package "WCT1012 15W Single coil Tx V3.1" is no longer open to public on website. But you can submit a request for the firmware package, NXP will evaluate your request based on business and determine if they send the package to you or not.

BR

XiangJun Rong

0 件の賞賛
返信