Disable interrupt during step CWHC08 V5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable interrupt during step CWHC08 V5

Jump to solution
2,489 Views
calou
Contributor III
Hello,
 
I use CW for HC08 and the evaluation freescale card with 9s08AW60. Is it possible in the debugger to disable interrupt during step?
 
Thank you very much
 
Regards
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,587 Views
Nabla69
Contributor V
Yes it is,
 
Simply double click on the "I" bit in the CCR Register and it will mask all maskable interrupt sources.
 
Cheers,
Alvin.

View solution in original post

0 Kudos
Reply
1 Reply
1,588 Views
Nabla69
Contributor V
Yes it is,
 
Simply double click on the "I" bit in the CCR Register and it will mask all maskable interrupt sources.
 
Cheers,
Alvin.
0 Kudos
Reply