Setting Output Compare with MC9S12C32

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Setting Output Compare with MC9S12C32

跳至解决方案
2,577 次查看
maurix1966
Contributor I
Hello!
 
I'm new with Freescale.
I've a problem with a MC9C12C32.
The question is:
how i can set , with processor expert, a pin to be an output compare?
 
I've tried with Processor Expert and i can only set a pin to be an Input Capture but not Output Compare.
 
Thank you for help.
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,770 次查看
CrasyCat
Specialist III
Hello
 
I have created a project for HCS12C32 and if I add a "TimeOut" Bean, I am able to define PT0_PWM0_IOC0 as output pin.
 
I am using CodeWarrior for HC12 V4.5
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,771 次查看
CrasyCat
Specialist III
Hello
 
I have created a project for HCS12C32 and if I add a "TimeOut" Bean, I am able to define PT0_PWM0_IOC0 as output pin.
 
I am using CodeWarrior for HC12 V4.5
 
CrasyCat
0 项奖励
回复