Disable interrupt during step CWHC08 V5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Disable interrupt during step CWHC08 V5

跳至解决方案
1,927 次查看
calou
Contributor III
Hello,
 
I use CW for HC08 and the evaluation freescale card with 9s08AW60. Is it possible in the debugger to disable interrupt during step?
 
Thank you very much
 
Regards
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,025 次查看
Nabla69
Contributor V
Yes it is,
 
Simply double click on the "I" bit in the CCR Register and it will mask all maskable interrupt sources.
 
Cheers,
Alvin.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,026 次查看
Nabla69
Contributor V
Yes it is,
 
Simply double click on the "I" bit in the CCR Register and it will mask all maskable interrupt sources.
 
Cheers,
Alvin.
0 项奖励
回复