Debugger broken for assembly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger broken for assembly

ソリューションへジャンプ
1,840件の閲覧回数
bob_walker
Contributor III

I've lost the ability to single step with the debugger in CW10.6, XP-SP3, 9S08SH16 target, Pemicro USBML-Universal. I've re-installed CW10.6 to no avail.

I can step with the debugger, and at times, it jumps to some arbitrary location. Note: NO INTERRUPTS on the target are enabled. When I do single step, it behaves correctly - most of the time

except for the previously cited jump to oblivion. However, when I run the code and then inspect buffers to verify data integrity - nada - it's all 0's. It's as if the debugger pod is not even retrieving data or updating the views at the breakpoint.

Furthermore, when I force an update - nothing. I've already lost 2 days on this and I cannot afford to lose any more time. Has anyone else had this much trouble with the debugger?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,717件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Bob.

this problem has to be checked with your project,  please upload it here, we can check.

Best Regards,

Zhang Jun

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,718件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Bob.

this problem has to be checked with your project,  please upload it here, we can check.

Best Regards,

Zhang Jun

0 件の賞賛
返信