Debugger broken for assembly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugger broken for assembly

Jump to solution
1,761 Views
bob_walker
Contributor III

I've lost the ability to single step with the debugger in CW10.6, XP-SP3, 9S08SH16 target, Pemicro USBML-Universal. I've re-installed CW10.6 to no avail.

I can step with the debugger, and at times, it jumps to some arbitrary location. Note: NO INTERRUPTS on the target are enabled. When I do single step, it behaves correctly - most of the time

except for the previously cited jump to oblivion. However, when I run the code and then inspect buffers to verify data integrity - nada - it's all 0's. It's as if the debugger pod is not even retrieving data or updating the views at the breakpoint.

Furthermore, when I force an update - nothing. I've already lost 2 days on this and I cannot afford to lose any more time. Has anyone else had this much trouble with the debugger?

Labels (1)
0 Kudos
Reply
1 Solution
1,638 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Bob.

this problem has to be checked with your project,  please upload it here, we can check.

Best Regards,

Zhang Jun

View solution in original post

0 Kudos
Reply
1 Reply
1,639 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Bob.

this problem has to be checked with your project,  please upload it here, we can check.

Best Regards,

Zhang Jun

0 Kudos
Reply