DEBUG ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEBUG ERROR

Jump to solution
2,253 Views
edigs
Contributor I


Hi there i have instaled CODEWARRIOR 10.4 special edition and at the debug section, the program had comed up with such an error. I would be very glad if someone could help me Thank you.

 

5074_5074.JPGCodeworrior error.JPG

Labels (1)
1 Solution
2,093 Views
TICS_Fiona
NXP Employee
NXP Employee

Please check whether the C code size is beyond the limit of your license.  Or did you enable C++ feature in your project? C++ language is only supported in professional edition. Please disable the C++ settings of the project as  below:

Cpp.png

View solution in original post

0 Kudos
Reply
3 Replies
2,094 Views
TICS_Fiona
NXP Employee
NXP Employee

Please check whether the C code size is beyond the limit of your license.  Or did you enable C++ feature in your project? C++ language is only supported in professional edition. Please disable the C++ settings of the project as  below:

Cpp.png

0 Kudos
Reply
2,093 Views
edigs
Contributor I

Thank you it work´s like a charm :smileygrin: 

2,093 Views
BlackNight
NXP Employee
NXP Employee

The message indicates that you your exceeding the allowed download size for your license configuration. Are you using the free edition?

And: are you using C++ (intentionally or unintentionally)?

See Please Check Your License | MCU on Eclipse

Hope this helps.

0 Kudos
Reply