DEBUG ERROR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,324件の閲覧回数
edigs
Contributor I


Hi there i have instaled CODEWARRIOR 10.4 special edition and at the debug section, the program had comed up with such an error. I would be very glad if someone could help me Thank you.

 

5074_5074.JPGCodeworrior error.JPG

ラベル(1)
1 解決策
2,164件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Please check whether the C code size is beyond the limit of your license.  Or did you enable C++ feature in your project? C++ language is only supported in professional edition. Please disable the C++ settings of the project as  below:

Cpp.png

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,165件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Please check whether the C code size is beyond the limit of your license.  Or did you enable C++ feature in your project? C++ language is only supported in professional edition. Please disable the C++ settings of the project as  below:

Cpp.png

0 件の賞賛
返信
2,164件の閲覧回数
edigs
Contributor I

Thank you it work´s like a charm :smileygrin: 

2,164件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The message indicates that you your exceeding the allowed download size for your license configuration. Are you using the free edition?

And: are you using C++ (intentionally or unintentionally)?

See Please Check Your License | MCU on Eclipse

Hope this helps.

0 件の賞賛
返信