Codewarrior 10.3 on Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 10.3 on Linux

ソリューションへジャンプ
24,132件の閲覧回数
bob_walker
Contributor III

When will CW10.3 be released for Linux?

ラベル(1)
1 解決策
16,368件の閲覧回数
BlackNight
NXP Employee
NXP Employee

There are no plans for 10.3 and Linux. Alternatives on Linux are CodeRed or Cocox.

元の投稿で解決策を見る

0 件の賞賛
返信
30 返答(返信)
4,174件の閲覧回数
tassiloböhr
Contributor I

Erich Styger schrieb:

There are no plans for 10.3 and Linux. Alternatives on Linux are CodeRed or Cocox.

So there is no chance anymore to code and debug HCS08 devices under linux with an up-to-date ide / toolchain?

Tassilo

0 件の賞賛
返信
4,174件の閲覧回数
cicero_ribeiro
Contributor I

can I find download link for codewarrior ide 10.2 for linux ?

Thanks.

0 件の賞賛
返信
4,174件の閲覧回数
Monica
Senior Contributor III

Cicero, here is the page where you can find the many editions and updates for CodeWarrior.

Regards!

CodeWarrior Downloads

0 件の賞賛
返信
4,174件の閲覧回数
Monica
Senior Contributor III

More specifically, you can find 10.2 and 10.3 versions right here under the "Software Development Tools" tab! CodeWarrior for MCU. Enjoy everyone!

0 件の賞賛
返信
4,174件の閲覧回数
cicero_ribeiro
Contributor I

Thanks for reply Monica,

But I can't see any version for linux.......    :smileysad:

Maybe you talk about  Power Architecture Eclipse Software

but I'm looking for s08 microcontrollers.

0 件の賞賛
返信
4,174件の閲覧回数
Monica
Senior Contributor III

Cicero, the Linux hosted Software is being uploaded in this very moment. You'll be able to see it there tomorrow (10.2)

Please let me know if you need anything else!

4,174件の閲覧回数
cicero_ribeiro
Contributor I

Thanks Monica.

0 件の賞賛
返信
4,174件の閲覧回数
bob_walker
Contributor III

Are you saying that Freescale has abandoned any and all tools that run on the Linux platform?!

CW10.2 is the LAST version for Linux?!

If this is the case, then WHAT is the reason for dropping Linux and where did this mandate come from?

0 件の賞賛
返信
4,174件の閲覧回数
JimDon
Senior Contributor III

Just codewarrior. Freescale supports many BSPs and tools on linux, just not  codewarrior any more.

If you had purchased a license, you may be able to get a refund.

0 件の賞賛
返信
4,174件の閲覧回数
bob_walker
Contributor III

I see. So in order to use Codewarrior 10.3 we will need to purchase a Microsoft license for Winxxx instead of using our Linux machines which worked just fine with Codewarrior 10.2.

If Freescale cannot support our platform of choice, then we will no longer support Freescale (i.e. no more Freescale designs.). Our company does not do Windows due to the security risks associated with that OS.