CodeWarrior MCU Updates

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior MCU Updates

1,510件の閲覧回数
romainbenet
Contributor III

Hi,

 

I need to get a file from NXP which indicates, for the CodeWarrior 10.6, all updates avalaibles with all modifications for each update with the previous.

 

Can someone find this (or these) document(s) please?

 

Best regards,

Romain

ラベル(1)
0 件の賞賛
返信
1 返信

1,398件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Romain,

It seems that there isn't the DOC, while you can checked the updates on the CW web:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

And for now , you can install the lasted version CW10.6.4, then install the lasted update 6,

then it can cover all of  the updates .

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

pastedImage_1.png

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信