CodeWarrior MCU Updates

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior MCU Updates

1,456 Views
romainbenet
Contributor III

Hi,

 

I need to get a file from NXP which indicates, for the CodeWarrior 10.6, all updates avalaibles with all modifications for each update with the previous.

 

Can someone find this (or these) document(s) please?

 

Best regards,

Romain

Labels (1)
0 Kudos
Reply
1 Reply

1,344 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Romain,

It seems that there isn't the DOC, while you can checked the updates on the CW web:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

And for now , you can install the lasted version CW10.6.4, then install the lasted update 6,

then it can cover all of  the updates .

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

pastedImage_1.png

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply