CodeWarrior HC08 v5.1 startup problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior HC08 v5.1 startup problem

ソリューションへジャンプ
4,072件の閲覧回数
What_lezhich
Contributor I
Hello People,
 
I have installed the CodeWarrior without any problems.
When I turn on the program I get a startup window in which I choose the "Create Project" button, afterwards,  I choose the MCU I use, at the next window I choose the language and the project's destination, when I push the "Next" button, the system crushes and "kicks" me out by turning itself off.
Also, by pushing the "Run Getting Started Tutorial" button at the startup window, I am getting the same results...
I tried to install the software at other computer and there were no problems. 
 
Does anybody know what may be the reason for such effect and how do I solve this task?
Thank you in advance.   
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,621件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
The search is at the bottom of this webpage :smileyhappy:

When searching for Groove, here's a direct link with the Groove bug workaround:

http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...

Given your description I don't have the impression it is the Groove incompatibility though.
Which os are you using, you did not mention it AFAIS.

And CW for MCU's 6.1 can be downloaded from www.freescale.com, download the "Special Edition".

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,621件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Which OS are you using?
There are compatibility issues with Microsoft's Groove, part of Microsoft's office tools. Do you have them installed, if so seach this forum for the workaround.
Also does the current CW for MCU's 6.1 behave better, did you try that current version?
Did you get any dump files?

Daniel
0 件の賞賛
返信
2,621件の閲覧回数
What_lezhich
Contributor I
Hi,
 
I'm sorry but I have no idea about where should I check for those installed "compatibility issues with Microsoft's Groove". I would be greatful if you could guide me where to search.
About the 6.1 version, I dont have it. All I have is the version I got from my university (v5.1). Also, would you tell me where I can get one (IF I can get one)?
 
Thanks alot,
Oleg.  
0 件の賞賛
返信
2,622件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
The search is at the bottom of this webpage :smileyhappy:

When searching for Groove, here's a direct link with the Groove bug workaround:

http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...

Given your description I don't have the impression it is the Groove incompatibility though.
Which os are you using, you did not mention it AFAIS.

And CW for MCU's 6.1 can be downloaded from www.freescale.com, download the "Special Edition".

Daniel
0 件の賞賛
返信
2,621件の閲覧回数
What_lezhich
Contributor I
Allrighty....!!!!! :smileywink:
 
All I had to do is to uncheck the "Run this program in compatibility mode for" in the compatibility tab of IDE.exe properties (like it was said in the link you gave me). From now and on, the program works like a Swiss watch :smileyhappy:
Thank you very much for your help, Daniel.
 
 
0 件の賞賛
返信