CodeWarrior HC08 v5.1 startup problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior HC08 v5.1 startup problem

跳至解决方案
3,089 次查看
What_lezhich
Contributor I
Hello People,
 
I have installed the CodeWarrior without any problems.
When I turn on the program I get a startup window in which I choose the "Create Project" button, afterwards,  I choose the MCU I use, at the next window I choose the language and the project's destination, when I push the "Next" button, the system crushes and "kicks" me out by turning itself off.
Also, by pushing the "Run Getting Started Tutorial" button at the startup window, I am getting the same results...
I tried to install the software at other computer and there were no problems. 
 
Does anybody know what may be the reason for such effect and how do I solve this task?
Thank you in advance.   
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,638 次查看
CompilerGuru
NXP Employee
NXP Employee
The search is at the bottom of this webpage :smileyhappy:

When searching for Groove, here's a direct link with the Groove bug workaround:

http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...

Given your description I don't have the impression it is the Groove incompatibility though.
Which os are you using, you did not mention it AFAIS.

And CW for MCU's 6.1 can be downloaded from www.freescale.com, download the "Special Edition".

Daniel

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,638 次查看
CompilerGuru
NXP Employee
NXP Employee
Which OS are you using?
There are compatibility issues with Microsoft's Groove, part of Microsoft's office tools. Do you have them installed, if so seach this forum for the workaround.
Also does the current CW for MCU's 6.1 behave better, did you try that current version?
Did you get any dump files?

Daniel
0 项奖励
回复
1,638 次查看
What_lezhich
Contributor I
Hi,
 
I'm sorry but I have no idea about where should I check for those installed "compatibility issues with Microsoft's Groove". I would be greatful if you could guide me where to search.
About the 6.1 version, I dont have it. All I have is the version I got from my university (v5.1). Also, would you tell me where I can get one (IF I can get one)?
 
Thanks alot,
Oleg.  
0 项奖励
回复
1,639 次查看
CompilerGuru
NXP Employee
NXP Employee
The search is at the bottom of this webpage :smileyhappy:

When searching for Groove, here's a direct link with the Groove bug workaround:

http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=1143&query.id=3988...

Given your description I don't have the impression it is the Groove incompatibility though.
Which os are you using, you did not mention it AFAIS.

And CW for MCU's 6.1 can be downloaded from www.freescale.com, download the "Special Edition".

Daniel
0 项奖励
回复
1,638 次查看
What_lezhich
Contributor I
Allrighty....!!!!! :smileywink:
 
All I had to do is to uncheck the "Run this program in compatibility mode for" in the compatibility tab of IDE.exe properties (like it was said in the link you gave me). From now and on, the program works like a Swiss watch :smileyhappy:
Thank you very much for your help, Daniel.
 
 
0 项奖励
回复