Code Warrior for QG8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior for QG8

Jump to solution
2,441 Views
admin
Specialist II
Hi everyone,
Can anyone suggest what is the correct compiler that I need to program the QG8?
Currently I have downloaded the

Special Edition: CodeWarrior for Microcontrollers 
Code Size Restriction:
HC(S)08/RS08 - 32K
ColdFire V1 - 64K

Would be very much appreciated if someone can put me on the right track.

Thanks!
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,525 Views
peg
Senior Contributor IV
Hi Learner,

Yes, Codewarrior for Microcontrollers Version 6.1 contains Freescales latest and greatest compiler for this device.

View solution in original post

0 Kudos
Reply
1 Reply
1,526 Views
peg
Senior Contributor IV
Hi Learner,

Yes, Codewarrior for Microcontrollers Version 6.1 contains Freescales latest and greatest compiler for this device.

0 Kudos
Reply