CW5.1, RS08 and Full Chip Simulation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW5.1, RS08 and Full Chip Simulation

ソリューションへジャンプ
4,968件の閲覧回数
Curt
Contributor IV
When I try to do a full chip simulation of an 'RS08 using CW5.1, the simulator reports 
that memory locations $221 (PTAPUD) and $222 (PTASE) -- as seen through the paging window -- are not implemented.  (Location $220 (PTAPE) _is_, however.) 
 
Certainly, the _simulator_ doesn't care about and of these three locations.  I _do_ though, since my code needs to initialize these locations if I want pull ups and the alleged slew rate protections.
 
So my question is:  is this just a problem on my CW installation, or is it part of some clever plan by the simulator makers?  
 
Has anyone else experienced this problem? 
 
Thanks in advance,
Curt
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,259件の閲覧回数
Curt
Contributor IV
The support people were unable to duplicate my problem (although I suspect that they did not try very hard). 
 
On a hunch though, I downloaded a CW service pack CW08_V5_KA1_SP.exe from the Freescale website and installed it.   This made my problem go away.
 
I think there must be bugs in my installation CD, which is 770-20997 REV B or
CWX-H08-SE REV. G depending on whether you use the number on the CD or the number on the box...:smileysad:
 
Anyway...  pass it along in case others may have similar difficulties.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,259件の閲覧回数
peg
Senior Contributor IV
Hi Curt,
 
You could also try taking it up with P&E Micro directly on their forum at www.pemicro.com
 
3,259件の閲覧回数
Curt
Contributor IV
Thanks.  I submitted a support request.
I'm starting to feel a little like a beta tester here:smileytongue:  Great fun though...
Can't believe I'm the first to run into this issue.  It's probably discussed at length somewhere in the docs (which are quite good ATC).
0 件の賞賛
返信
3,260件の閲覧回数
Curt
Contributor IV
The support people were unable to duplicate my problem (although I suspect that they did not try very hard). 
 
On a hunch though, I downloaded a CW service pack CW08_V5_KA1_SP.exe from the Freescale website and installed it.   This made my problem go away.
 
I think there must be bugs in my installation CD, which is 770-20997 REV B or
CWX-H08-SE REV. G depending on whether you use the number on the CD or the number on the box...:smileysad:
 
Anyway...  pass it along in case others may have similar difficulties.
0 件の賞賛
返信
3,259件の閲覧回数
CrasyCat
Specialist III
Hello
 
This seems to be an issue in the RS08 simulator.
You need to submit a service request  for that.
 
To log the issue please go to following URL:
    http://www.freescale.com/TechSupport
and click on "Submit a service request"
 
CrasyCat