CW+PEMicro Multilink in Ubuntu 14.04 64bits

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW+PEMicro Multilink in Ubuntu 14.04 64bits

3,517 次查看
almirbraggio
Contributor I

Hello,
I have tried using the CW on Ubuntu 14.04 LTS 64 bits.

The installation was apparently a success.

20573_20573.pngScreenshot from 2015-03-06 13_09_50.png

I'm trying to program MCF51JM32 using the PEMicro Multilink Universal. Driver PemicroLinuxDrivers_2015_02_02.

The error is seen in this screenshot.

20574_20574.pngScreenshot from 2015-03-06 13_15_10.png

The log console:

=== CodeWarrior GDI protocol log ===

GDI DLL: /opt/Freescale/CodeWarrior_MCU_10.2/MCU/CodeWarrior/CodeWarrior_Plugins/Debugger/Protocols/../../Support/ColdFire/gdi/cf_pne_gdi.so

CPU: MCF51JM32

GDI: DiGdiOpen()

GDI: => DI_ERR_FATAL

GDI: The Debugger can not reset the connected hardware.

GDI: DiGdiOpen()

GDI: => DI_ERR_FATAL

GDI: The Debugger can not reset the connected hardware.


Can anyone help me? Codewarrior for Linux has not been good. Only works on Ubuntu 10... =S

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

3,120 次查看
almirbraggio
Contributor I

The best solution: Virtualbox.

Cheers,

Almir Braggio

0 项奖励
回复

3,120 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Almir,

per CW10.2 system requirement, it can support Ubuntu 10.04 only. it wasn't tested under Ubuntu 14.04.

So officially CW10.2 doesn't support Ubuntu 14.04.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,120 次查看
almirbraggio
Contributor I

Hello, ZhangJennie,

So officially unsupported. But there are possibilities, right?
It would be interesting to list the dependencies and their versions to run on other versions of Ubuntu.
I am limited to one OS version.


Best regards,

Almir Braggio

0 项奖励
回复