CW+PEMicro Multilink in Ubuntu 14.04 64bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW+PEMicro Multilink in Ubuntu 14.04 64bits

2,442件の閲覧回数
almirbraggio
Contributor I

Hello,
I have tried using the CW on Ubuntu 14.04 LTS 64 bits.

The installation was apparently a success.

20573_20573.pngScreenshot from 2015-03-06 13_09_50.png

I'm trying to program MCF51JM32 using the PEMicro Multilink Universal. Driver PemicroLinuxDrivers_2015_02_02.

The error is seen in this screenshot.

20574_20574.pngScreenshot from 2015-03-06 13_15_10.png

The log console:

=== CodeWarrior GDI protocol log ===

GDI DLL: /opt/Freescale/CodeWarrior_MCU_10.2/MCU/CodeWarrior/CodeWarrior_Plugins/Debugger/Protocols/../../Support/ColdFire/gdi/cf_pne_gdi.so

CPU: MCF51JM32

GDI: DiGdiOpen()

GDI: => DI_ERR_FATAL

GDI: The Debugger can not reset the connected hardware.

GDI: DiGdiOpen()

GDI: => DI_ERR_FATAL

GDI: The Debugger can not reset the connected hardware.


Can anyone help me? Codewarrior for Linux has not been good. Only works on Ubuntu 10... =S

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,045件の閲覧回数
almirbraggio
Contributor I

The best solution: Virtualbox.

Cheers,

Almir Braggio

0 件の賞賛
返信

2,045件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Almir,

per CW10.2 system requirement, it can support Ubuntu 10.04 only. it wasn't tested under Ubuntu 14.04.

So officially CW10.2 doesn't support Ubuntu 14.04.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,045件の閲覧回数
almirbraggio
Contributor I

Hello, ZhangJennie,

So officially unsupported. But there are possibilities, right?
It would be interesting to list the dependencies and their versions to run on other versions of Ubuntu.
I am limited to one OS version.


Best regards,

Almir Braggio

0 件の賞賛
返信