CODEWARRIOR 10.5 issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CODEWARRIOR 10.5 issues

2,092件の閲覧回数
Braulio_Cespede
Contributor III

Hello Everyone, I was trying to build a Project in Codewarrior 10.5, then suddenly this happen:

10289_10289.jpgcodewarrior issues.JPG.jpg

As you can see, the build do not go more than 10%.

I dont know what is happening. I think, It could be the Compiler, but I dont know how to chance it.

 

Thanks for Advanced.

 

Note:

I had noticed that If I try with another project there's no problem, It's build the project.

Apparently It's just happening in the "My Star Network Demo (End Device)" project for MC13234C (Wireless tranceiver).

 

Update:

I managed to solve the problem, I will post the solution later.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,911件の閲覧回数
dmarks_ls
Senior Contributor II

It looks like perhaps it's getting stuck on the pre-build step.  What appears in the Console window when you try to build?  (The tab for the Console is next to Problems.)

0 件の賞賛
返信

1,911件の閲覧回数
Braulio_Cespede
Contributor III

Thanks for Answer.

Look:

codewarrior issues2.JPG.jpg

0 件の賞賛
返信

1,911件の閲覧回数
Robinwithu
Senior Contributor I

Hi,

does it's showing anything on Problem window??

Thanks n Regards,

Robin

0 件の賞賛
返信

1,911件の閲覧回数
Braulio_Cespede
Contributor III

Nope, Nothing.

Also, the problem is the same for CW 10.4.

I had noticed that If I try with another project there's no problem, It's build the project.

Apparently It's just happening in the "My Star Network Demo (End Device)" project for MC13234 (Wireless tranceiver).

0 件の賞賛
返信