Board Level Bringup using CodeWarrior TAP and GDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Board Level Bringup using CodeWarrior TAP and GDB

2,148 Views
michaelmeier
Contributor II

It is with great interest that I watched this video:

http://www.nxp.com/video/board-level-bringup-using-codewarrior-tap-and-gdb:BOARDLVL_CWTAPGDB_VID

 

Around 1:56 the speaker says:

"If you're not exactly thrilled with how we did the GDB server, no problem. It's open source and you can get it from us, for free. Just ask us. Let's work together."

 

Where can I get it from? Who do I have to ask?

Labels (1)
0 Kudos
Reply
2 Replies

1,773 Views
wtoner
Contributor I

Is that video still available somewhere? I would like to view it.

0 Kudos
Reply

1,773 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Michael Meier,

Currently the feature of bringing up the target board with CodeWarrior and GDB is not open in the public Website, if you are interested in it, you could create a ticket to require the related documents and packages.

Please refer to this thread about how to create a service request How I could create a Service Request? .


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply