Board Level Bringup using CodeWarrior TAP and GDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Board Level Bringup using CodeWarrior TAP and GDB

2,149件の閲覧回数
michaelmeier
Contributor II

It is with great interest that I watched this video:

http://www.nxp.com/video/board-level-bringup-using-codewarrior-tap-and-gdb:BOARDLVL_CWTAPGDB_VID

 

Around 1:56 the speaker says:

"If you're not exactly thrilled with how we did the GDB server, no problem. It's open source and you can get it from us, for free. Just ask us. Let's work together."

 

Where can I get it from? Who do I have to ask?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,774件の閲覧回数
wtoner
Contributor I

Is that video still available somewhere? I would like to view it.

0 件の賞賛
返信

1,774件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Michael Meier,

Currently the feature of bringing up the target board with CodeWarrior and GDB is not open in the public Website, if you are interested in it, you could create a ticket to require the related documents and packages.

Please refer to this thread about how to create a service request How I could create a Service Request? .


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信