10.5 to 10.6 -> behavior changed, s-file changed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

10.5 to 10.6 -> behavior changed, s-file changed

893 次查看
andreasvogt
Contributor I

Hi to everyone,

 

I compiled the same project (every project file and source file is identically) on CW10.5 and CW10.6. The result is that I have two different s-files and the code behaves differently. In the new 10.6 MAP file the size of different locations changed.

 

Made someone the same experience? What changed between 10.5 and 10.6?

标签 (1)
0 项奖励
回复
1 回复

823 次查看
trytohelp
NXP Employee
NXP Employee

Hi Andreas,

The build tool chain was updated so depending of your project, the generated code could be different and so the Srecord file and project mapping too.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------