Hi,
the eGUI and TWR-LCD i recommended integrated display RAM and simple serial peripheral interface (SPI) or parallel bus interface. The eGUI supports conventional LCD panels and ColdFire LCD MPUs.
we also have (TWR-LCD-RGB) adds a side mounting TFT WQVGA Display to the Freescale Tower System. It can be used with Tower Processor Modules featuring an RGB interfacing LCD Controller. but it doesn't support CF V1.
CW integrates LCD bean which works for 8/16bit MCU and CFV1, but it is for segment display. from what i know, there is no other pe component to implement full LCD function.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------