usbtap driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usbtap driver

1,183 Views
gangqunshen
Contributor I

it can't automatic load the usbtap drive in windows10 OS(x64) when i plug in the usbtap. the codewarrior version is as follow pic:

155716_155716.pngpastedImage_0.png

i also try to manual load the drive which searching the whole Freescale folder, but still can't find the right driver.

does someone has the same problem?

what should i do?

thanks a lot.

Labels (1)
0 Kudos
Reply
1 Reply

1,078 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Gangqun

CodeWarrior for MCU v10.6.4 is not verified under support Windows 10. It only supports:

Microsoft® Windows XP 32-bit and 64-bit (Professional Edition)

Microsoft Windows 7 32-bit and 64-bit (Home Premium Edition and Professional Edition)

Microsoft Windows 8 32-bit and 64-bit (Home Premium Edition and Professional Edition)

For details, please review this page:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply