usbtap driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usbtap driver

1,094件の閲覧回数
gangqunshen
Contributor I

it can't automatic load the usbtap drive in windows10 OS(x64) when i plug in the usbtap. the codewarrior version is as follow pic:

155716_155716.pngpastedImage_0.png

i also try to manual load the drive which searching the whole Freescale folder, but still can't find the right driver.

does someone has the same problem?

what should i do?

thanks a lot.

ラベル(1)
0 件の賞賛
返信
1 返信

989件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Gangqun

CodeWarrior for MCU v10.6.4 is not verified under support Windows 10. It only supports:

Microsoft® Windows XP 32-bit and 64-bit (Professional Edition)

Microsoft Windows 7 32-bit and 64-bit (Home Premium Edition and Professional Edition)

Microsoft Windows 8 32-bit and 64-bit (Home Premium Edition and Professional Edition)

For details, please review this page:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信