CodeWarrior Development Tools Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior Development Tools Knowledge Base

Labels

Discussions

Sort by:
This project is an example of using the DSC CodeWarrior linker to place code in a different area of memory.  In this case, the FlexNVM flash block is used. The example uses three different methods in the linker command file to force specific code to a different memory segment, see examples below.  For more information on the linker syntax, see the manual installed with CodeWarrior at \CW MCU v10.6.x\MCU\Help\PDF\MCU_DSC_Compiler.pdf     This project was developed for the TWR-56F8400 Tower development board, using CodeWarrior for Microcontrollers v10.6.6.  The project was created using Processor Expert, and blinks an LED using the PIT timer interrupt.     The linker command file is located at \Project_Settings\Linker_Files\FLASH_SDM.cmd.Here are the key changes to the project:     MEMORY {         # Added .p_FlexNVM memory segment         .p_FlexNVM(RWX) : ORIGIN = 0x00068000, LENGTH = 0x00004000 }     # Added .FlexNVM_Code memory section .FlexNVM_Code : {   TI1_c.obj (.text) # Place whole source file in this section   OBJECT (FPE_low_level_init, cpu_c.obj) # Place individual function in this section   * (FlexNVM_code.text) # Place from section defined in source code, see main.c     } > .p_FlexNVM     and in main.c: #pragma define_section FlexNVM_code "FlexNVM_code.text"  RX #pragma section FlexNVM_code begin void main(void) {   /* Write your code here */ } #pragma section FlexNVM_code end
View full article
In some of the post I've talked about the many advantages that the combination CodeWarrior-Eclipse can bring up. One of those was the installation on service Packs in a friendlier way than when it's done with the classical view of CodeWarrior. That is why I introduce today the Installing Service Pack for CodeWarrior Tools Quick Start   This Quick Start, in case you are choosing the hard and equally great way to do your own thing with CodeWarrior, it explains how to install a service pack or an update for your classical version of the software running on the Windows platform.   It shows step by step how to do this manually and correctly, preventing you from having an IDE full of stuff you don't even want to use.
View full article
  It's true, coding isn't always an easy job, specially when it comes to tools you are not familiar with. I'm not an expert atCodeWarrior, but I really enjoy developing embedded systems or at least parts of them. Obviously, there will be a bunch of error messages depicting on the IDE at the beginning. (great feature for some, altough C and C++ don't show lexic nor command mistakes right away).   While trying to pull off a set of code lines I had been working on, there usually come along a bunch of funy error messages deploying, such as  "illegal 'friend' declaration" or "function has no prototype".   Well, I recently found an updated  BUILD TOOLS MESSAGE REFERENCE MANUAL at Freescale's web page. The Build Tools Message Reference Manual documents the messages generated by your CodeWarrior build tools. This information helps you fix problems the build tools encounter as they build your projects. Note that this manual documents just those messages that are generated by compiler, assembler, and linker.   It shows a broad list of error messages and how to fix them, so go check it now, useful as it can be!
View full article
Hey there! Are you familiar with this device shown on top? If you find it similar to the CodeWarrior TAP probe then you are ringing the right bells.   The magic thing of this innovative device is that you can debug systems remotely or more effectively share a single system with multiple developers. When a shared system is not needed, CodeWarrior TAP connects directly to the developer’s workstation with a single USB cable. Power is supplied by the USB port so that no additional cables are required!   This means that the TAP also enables Freescale target system debugging via a standard debug port (usually JTAG) while being connected to your workstation via Ethernet or USB. For this reason this device can also be found under the name of probe, JTAG probe, JTAG emulator or target probe.   These are some of the great features offered by the TAP: Allows either USB or Ethernet (10/100 ) host connection for the developer workstation USB powered, even when using Ethernet Low cost removable probe tips sold separately Supports debugging via JTAG interface Automatically supports system voltage levels from 1.2 to 3.3 Supports all available core speeds and voltages for supported Freescale processors As a convenience feature, the CodeWarrior can connect to a target systems serial port allowing telnet access to a remotely located system and control of the U-boot program.   Keep finding more features and applications within the Fact Sheet If you'd like to dig further into the TAP world, you can also find The User Guide equally useful!      Please note that this device is not up for sale (just yet!). Regardless, Freescale is accepting pre-orders for CodeWarrior TAP now with shipments planned in late October, and DebuggerGuys will keep you informed on this! Don't hesitate on asking beyond!      
View full article
The content is to tell user how to add nand flash(MT29F2G08ABBDA) support in CW 10.3.
View full article
CodeWarrior MCU 10.5 for Kinetis KV10   To setup your CodeWarrior development environment for Kinetis KV10 applications. Read the documents attached for download and installation instructions. Download and install the CW MCU v10.5  product, patch and service pack in the order specified:   Evaluation: CodeWarrior for Microcontrollers 10.5 (Eclipse, Offline) CW MCU v10.5 PEx MQX Lite Update 1.0.1 CW MCU v10.5 Kinetis KV10 75MHz Service Pack   the updates were just posted on the following URLs: http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_10_5
View full article
This Quick Start explains how to install service pack updater archive for your CodeWarrior software running on the Windows or Linux platform.   Support for new devices and/or updates can be added to the CodeWarrior Development Studio for Microcontrollers v10.x (CW MCU10.1) directly from the Internet (Online mode) or from a downloaded archive (Offline mode).   This document describes both the Offline and Online modes of updating CodeWarrior MCU v10.1 and a troubleshooting update. These instructions will show you how to manipulate that list to ensure that you can focus on the right URL for the CodeWarrior tools update.The topics covered in this document are:   • Updating Online: Lists the steps required to complete the update when you are connected to the Internet.   • Troubleshooting Updates:  Lists the troubleshooting updates.   • Updating Offline: Lists the steps required to complete the update when you are not connected to the Internet.   Start catching up with this updater archive!
View full article
The CodeWarrior USB TAP probe is a cost-effective tool that helps you develop and debug a number of processors and microcontrollers. This chapter introduces you to the USB TAP probe.   The USB TAP probe uses advanced emulation technology to provide control of and visibility into your target system. Combined with the CodeWarrior IDE, the USB TAP speeds the debugging process by letting you interactively control and examine the state of your target system.   The USB TAP probe has these features: • Supports the following systems: Power Architecture processors, StarCore processors, 56800 Hybrid Controllers (processors and microcontrollers), and ColdFire™ processors. • Supports all CPU core speeds. • Lets you control and debug software running in-target, with minimal intrusion into target operation. • Lets you debug code in cache, ROM, RAM, and flash memory. • Provides high performance: – Split-second single-step execution. – Capable of download speeds greater than 12 MB per minute from host to target.   ...and so much more!!! Get into the USB TAP probe world to make it easier and faster! Watch how over here.    
View full article
The CodeWarrior Ethernet TAP probe is a tool that helps you develop and debug a number of processors and microcontrollers.   The Ethernet TAP probe uses advanced emulation technology to provide control of and visibility into your target system. Combined with a host debugger, it speeds the debugging process by letting you interactively control and examine the state of your target system.   The Ethernet TAP probe has these features: • Supports the following systems: PowerPC™ processors, StarCore processors, ColdFire® processors, 56800 Hybrid Controllers (processors and microcontrollers), ARM® processors, and RCF base-band controllers. (All products reference at Freescale web page!) • Supports all CPU core speeds. • Lets you control and debug software running in-target, with minimal intrusion into target system operation. • Lets you debug code in cache, ROM, RAM, and flash memory. • Provides high performance: – Split-second single-step execution. – Capable of download speeds greater than 12 MB per minute from host to target system.   ...and many more of them! Get it updated today!!!      
View full article
To start expanding horizons in CodeWarrior, a great portfolio to use is definetely ColdFire, which houses 32-bit MCUs solutions.   Enabled by a vast ecosystem of development tools and design resources, development on 32-bit gets as easy as it can be!   After having the proper guidance on ColdFire projects, one of the most important things to do is to optimize devices as for speed and size. Not saying that it is completely necessary, but if you already have it, why not using it?   The following documentation is a complete guide to configure compiler options for optimal performance of ColdFire devices, and provides two sets of options to do this: One set optimizes speed; Another set optimizes code size.   Besides, the document contains two main forms of pulling this optimizations off: • MCU 10.x Eclipse IDE • Command Line   Both ways are functional if you want to configure compiler options for speed or size, it's up to you!   It's easily and quickly done, get a try of the application note here! Configuration
View full article
The SmartDSP Operating System (OS) is a Real Time Operating System (RTOS) that, in addition to providing drivers for the MSBA8100 processor, also runs on the following StarCore DSP-based processors: • PSC9131 • MSC815x/MSC825x • MSC814x • MSC812x • MSC8101/3 • MSC711x   The StarCore CodeWarrior (CW) Development Studio includes SmartDSP OS royalty-free source code. Further, SmartDSP OS has a high-level Application Programming Interface (API) that lets users develop integrated applications for StarCore processors.   In SmartDSP OS, most functions are written in ANSI C. However, when needed, Assembly optimizes time-critical functions by maximizing StarCore’s multiple execution units.   Other SmartDSP OS features include the following: • small memory footprint ideal for high-speed StarCore processors • priority-based event-driven scheduling (triggered by user applications or HW) • dual-stack pointer for exception and task handling • inter-task communication using queues, semaphores, and events.   And this is just the beginning of what you can do with SmartDSP OS, get updated here and start coding with DebuggerGuys!
View full article
The StarCore assembly language tools consist of an assembler, a linker, an archiver, and several utilities.   Freescale's DSP (Digital Signal Processors), built on StarCore technology, offer high-performance programmable devices for baseband, aerospace, defense, medical and test and measurement markets. The StarCore DSP portfolio provides customers with fully scalable and flexible solutions to get to market faster. Combine that with the low power and low cost of the StarCore DSPs and they are the ideal solution for your next design.   Today we're bringing up the Assembler User Guide that contains the walk-thrus of StarCore DSP Architectures on CodeWarrior Development Studio. This manual explains the assembly language tools for the StarCore DSP cores. As it is mentioned somewheren within the User Guide, the StarCore assembler architecture is compiler-friendly, so you can combine it with a compiler that generates exceptionally compact code.   With this great advantage, you can write applications in C, for example, yet achieve code density and high performance comparable to that of hand-coded assembly programs!   Get a glance at this manual and start using CodeWarrior for StarCore DSP today!   Don't be afraid and ask any questions to DebuggerGuys
View full article
I just download FNET2.5.0, it can't debug it by CW10.4, it comes error message when I start debug "Could not open memory configuration file".   The CW10.4 works for other examples project.   Why?   Regards Sam
View full article
The StarCore C/C++ compiler, in conjunction with the assembler and the linker, generates binaries for the StarCore family of DSP. Freescale's DSP (Digital Signal Processors), built on StarCore technology, offer high-performance programmable devices for baseband, aerospace, defense, medical and test and measurement markets. The StarCore DSP portfolio provides customers with fully scalable and flexible solutions to get to market faster. Combine that with the low power and low cost of the StarCore DSPs and they are the ideal solution for your next design. Today we're bringing up The StarCore C/C++ Compiler User Guide, which explains how to operate this compiler. In addition, thedocument describes you how to optimize C/C++ source code to let the compiler take full advantage of the StarCore processor’s advanced hardware. Awesome, isn't it? Multitask documentation like this make it easier and better to start programming! Get a glance at this manual and start using CodeWarrior for StarCore DSP today! Don't be afraid and ask any questions to DebuggerGuys
View full article
CodeWarrior Development Studio is a complete integrated Development Environment (IDE) that provides a highly visual and automated framework to accelerate the development of the most complex embedded applications.   I now present you a manual that describes the CodeWarrior IDE and debugger features that are common across all the CodeWarrior products, in which you can find many interesting things for people who's just starting to break down CodeWarrior great features.   Within the overview of this manual you will also find: • Release Notes • Documentation Structure • Manual Conventions • CodeWarrior IDE Overview   Download CodeWarrior and get to see the Reference Manual right away!  
View full article
The purpose of this document is to help understand and create Flash configuration files for the Flash Programming interface.   A Flash Configuration file is an XML format file. Its file extension is always “XML”. It is possible to open and edit this file with any text editor. This file is a “handmade” file and is not created automatically with any tool.   Some microcontrollers can address the flash in multiple ways ─ banked and paged. Therefore, multiple overlapping devices can be defined for one microcontroller. Each of them is defined in its own Flash Configuration XML file.   The *.XML files contain microcontroller- dependent parameters and applets to handle internal flash modules. Applets are small programs which are loaded into the on-chip RAM. They will run at well-defined speed (depending on the microcontroller clock speed) and can collect data about the state of the memory modules, can control the memory modules (including erasing and programming). There are three applets for each flash module: http://pcdn.500px.net/4130499/a271bcea97e80e8d223b3338b27c9f116cdd98a3/3.jpg• INFO applet ─ Collects information about the module. • CONTROL applet ─ Controls and erases the module. • PROGRAM applet ─ Programs the module.   Parameters are passed to these applets at fixed memory addresses, which are relative to the workspace. *.XML files are written by Freescale and are delivered within the installation.   Keep learning and pull off your own applet with this Application Note!
View full article
This manual explains how to use the CodeWarrior Development Studio tool set to develop software for Freescale StarCore DSP processors. Following now, we present you an overview of this manual as a little introduction to the CodeWarrior development tools and development process.   Before using the CodeWarrior IDE, this targeting manual recommends you to read the developer notes. These notes contain important information about last-minute changes, bug fixes, incompatible elements, or other sections that may not be included within the manual.   Programming for StarCore processors is much like programming for any other CodeWarrior platform target. If you have not used CodeWarrior tools before, start by studying the Eclipse IDE, which is used to host the tools.   If you are an experienced CodeWarrior user, note that the CodeWarrior Development Studio for StarCore DSP Architecture environment uses the Eclipse IDE and the interface is substantially different from the “classic” CodeWarrior IDE. But there's no reason to feel lost! The manual will give you the walk-thrus to become a skilled CodeWarrior programmer!   Start exploring the possibilities with this amazing development tool, what are you waiting for?  
View full article
How to use error directive in codewarrior version 10.6 as i am facing problem which is able to see in  attached sheet
View full article