problem with programming S08SH8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem with programming S08SH8

ソリューションへジャンプ
3,055件の閲覧回数
juliancox
Contributor V

Using CW11 and Multilink Universal I can debug my S08SH8 successfully, but when I try to flash program it i get the error

juliancox_0-1600880034139.pngjuliancox_0-1600880034139.png

Also when using the cyclone i get the Error Code $00000007 Error: Cannot enter debug mode.

I am not , and never have, used a MC9S08QE16

0 件の賞賛
返信
1 解決策
3,045件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

From your picture 

 

Are you are trying to program the SH or the QE device?

 

Please check that you only have one project open in code warrior also please check that the connection is for the SH device

I hope this will help you

 

Regards

Vicente

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,974件の閲覧回数
juliancox
Contributor V

I know this is a very old post, but I am just tidying up. However:

1. When I say that I am not, and have never used a QE16 - that is a clue to the fact that I am NOT trying to program a QE16

2. I have only one open project, but since none of my (closed) projects use  a QE16, whether I have all or only one project open should not matter.

0 件の賞賛
返信
3,046件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

From your picture 

 

Are you are trying to program the SH or the QE device?

 

Please check that you only have one project open in code warrior also please check that the connection is for the SH device

I hope this will help you

 

Regards

Vicente

 

0 件の賞賛
返信