multilink universal not being recognized

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

multilink universal not being recognized

1,795件の閲覧回数
haroldvogel
Contributor II

When I attempt to load the application on to my board in the debugger I receive:

118720_118720.pngpastedImage_0.png

I have unplugged and plugged in the USB connector to the multilink unit.

I have restarted the computer.

I have turned off the computer and restarted the computer.

I have powered off the board and disconnected the multilink unit powered the computer down and restarted the computer after the computer is up and running I connected the USB cable to the multilink device and powered the board back up with the same above result.

 

Hope you can tell me what is wrong.

 

John Vogel

ラベル(1)
0 件の賞賛
返信
1 返信

1,626件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi John,

It seems the interface is recognized as it's displayed in the P&E Connection Assistant.

Most of the time (from my experiences) I  met similar problem when the connection on board was wrong (wrong port).

Now if there is a problem with the P&E driver, on the P&E web site you will find some information which could help you but for me it's not the problem.

Please have a look to:

    P&E Microcomputer Systems

    P&E Microcomputer Systems

This morning I've performed some tests on my side.

The configuration used was:

    - Multilink Universal rev.B

    - TWR-K21D50M with TWR-ELEV

Test_1: Multilink plugged on PC -> not connected on board.

On Multilink only the led blue was lighted.

Here I got same message:

pastedImage_3.png

Test_2: Multilink plugged on PC -> connected to the board but board power off.

On Multilink only the led blue was lighted.

Launching the debug session, the same error appears.

Test_3: Multilink plugged on PC -> connected to the board and board power on.

On Multilink the leds blue and orange were lighted and the application is loaded on board.

pastedImage_7.png

For me you've a problem between the Multilink and board.

This could be due to wrong on-board port used or power supply.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信