multilink universal not being recognized

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

multilink universal not being recognized

1,791 Views
haroldvogel
Contributor II

When I attempt to load the application on to my board in the debugger I receive:

118720_118720.pngpastedImage_0.png

I have unplugged and plugged in the USB connector to the multilink unit.

I have restarted the computer.

I have turned off the computer and restarted the computer.

I have powered off the board and disconnected the multilink unit powered the computer down and restarted the computer after the computer is up and running I connected the USB cable to the multilink device and powered the board back up with the same above result.

 

Hope you can tell me what is wrong.

 

John Vogel

Labels (1)
0 Kudos
Reply
1 Reply

1,622 Views
trytohelp
NXP Employee
NXP Employee

Hi John,

It seems the interface is recognized as it's displayed in the P&E Connection Assistant.

Most of the time (from my experiences) I  met similar problem when the connection on board was wrong (wrong port).

Now if there is a problem with the P&E driver, on the P&E web site you will find some information which could help you but for me it's not the problem.

Please have a look to:

    P&E Microcomputer Systems

    P&E Microcomputer Systems

This morning I've performed some tests on my side.

The configuration used was:

    - Multilink Universal rev.B

    - TWR-K21D50M with TWR-ELEV

Test_1: Multilink plugged on PC -> not connected on board.

On Multilink only the led blue was lighted.

Here I got same message:

pastedImage_3.png

Test_2: Multilink plugged on PC -> connected to the board but board power off.

On Multilink only the led blue was lighted.

Launching the debug session, the same error appears.

Test_3: Multilink plugged on PC -> connected to the board and board power on.

On Multilink the leds blue and orange were lighted and the application is loaded on board.

pastedImage_7.png

For me you've a problem between the Multilink and board.

This could be due to wrong on-board port used or power supply.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply