how to modify I/O support to Debugger Console

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to modify I/O support to Debugger Console

2,336 Views
PO220
Contributor IV

Hi

 

I use CW 10.6 with MQXlite (Processor Expert).

The project is configured for I /0 support  UART (default) ; How can I change I / O support to debugger console ?

Create a new project and re-create all the  PE components seems impossible without errors !

 

Thank you in advance

Labels (1)
4 Replies

2,095 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Please tell me you use which chip .

BR

Alice

0 Kudos
Reply

2,095 Views
PO220
Contributor IV

Hello

it's a KL15Z128VLH4.

Thank you

0 Kudos
Reply

2,095 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

(1) If  you want to modify it when you create project , you can configure here :

pastedImage_0.png

(2) If you want to change it after create project , you can configure here :

pastedImage_1.png

we can configure it refer to this :

pastedImage_2.png


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,095 Views
PO220
Contributor IV

Thank you very much !

0 Kudos
Reply