how to modify I/O support to Debugger Console

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to modify I/O support to Debugger Console

1,700 次查看
PO220
Contributor IV

Hi

 

I use CW 10.6 with MQXlite (Processor Expert).

The project is configured for I /0 support  UART (default) ; How can I change I / O support to debugger console ?

Create a new project and re-create all the  PE components seems impossible without errors !

 

Thank you in advance

标签 (1)
4 回复数

1,459 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Please tell me you use which chip .

BR

Alice

0 项奖励
回复

1,459 次查看
PO220
Contributor IV

Hello

it's a KL15Z128VLH4.

Thank you

0 项奖励
回复

1,459 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

(1) If  you want to modify it when you create project , you can configure here :

pastedImage_0.png

(2) If you want to change it after create project , you can configure here :

pastedImage_1.png

we can configure it refer to this :

pastedImage_2.png


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,459 次查看
PO220
Contributor IV

Thank you very much !

0 项奖励
回复