error while compiling the SPC5643L crc project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

error while compiling the SPC5643L crc project

2,818 次查看
steven_zhang
Contributor V

i complier the CRC proget  following the https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/How-to-use-CRCgen-in-CodeWarrior-for-MCU/ta-p/11...

get the following error:

D:/Freescale/CW MCU v11.1/gnu/bin/mingw32-make --no-print-directory post-build
D:\Freescale\CW MCU v11.1\eclipse\../MCU/bin/crcgen.exe" "C:\Users\stevenzhang\workspace\test5643l_crc\FLASH/test5643l_crc.elf" -crc C:/Users/stevenzhang/workspace/test5643l_crc/Project_Settings/Linker_Files/calc_crc.crc" -srec "C:\Users\stevenzhang\workspace\test5643l_crc\FLASH/test5643l_crc.elf.crc.mot" 26
' '
'D:\Freescale\CW' 不是内部或外部命令,也不是可运行的程序
或批处理文件。----- it not an internal or external command。
mingw32-make[1]: [post-build] Error 1 (ignored)

how to fist the problem?

0 项奖励
回复
1 回复

2,424 次查看
stanish
NXP Employee
NXP Employee

Hi,

not sure if it's a copy&paste issue but there is missing quotation mark at the beginning of the line:

D:\Freescale\CW MCU v11.1\eclipse\../MCU/bin/crcgen.exe" 

I'd expect this:

"D:\Freescale\CW MCU v11.1\eclipse\../MCU/bin/crcgen.exe" 

 

Also the error message indicates the spaces in path is causing issue in parsing the string of the post process steps.

Hoe it helps.

Stan

0 项奖励
回复