debug without flashing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

debug without flashing

2,127件の閲覧回数
jaymoskowitz
Contributor I

Currently in Code Warrior (5.9.0), I select "Debug" in order to flash a new version of code. How can I use the debugger against code that it has already flashed if I wish to do another debug session a day or two later. Right now it is reflashing each time I select debug.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,056件の閲覧回数
jaymoskowitz
Contributor I

I am using an MCS12XD

0 件の賞賛
返信

2,056件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jay,

There is not the selection for this .

- While if you only want to debug , i think you can use the "Full chip simulation" to debug.

- And also you can configure the .prm file , place all of the code into RAM when your

code is small , (in this method, if the size code larger , the RAM not enough ).

Hope it helps

Alice

0 件の賞賛
返信

2,056件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jay,

Could you tell us which MCU are you using?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信