debug without flashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

debug without flashing

2,271 次查看
jaymoskowitz
Contributor I

Currently in Code Warrior (5.9.0), I select "Debug" in order to flash a new version of code. How can I use the debugger against code that it has already flashed if I wish to do another debug session a day or two later. Right now it is reflashing each time I select debug.

标签 (1)
0 项奖励
回复
3 回复数

2,200 次查看
jaymoskowitz
Contributor I

I am using an MCS12XD

0 项奖励
回复

2,200 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jay,

There is not the selection for this .

- While if you only want to debug , i think you can use the "Full chip simulation" to debug.

- And also you can configure the .prm file , place all of the code into RAM when your

code is small , (in this method, if the size code larger , the RAM not enough ).

Hope it helps

Alice

0 项奖励
回复

2,200 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jay,

Could you tell us which MCU are you using?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复