Will the classic CodeWarrior IDE work under windows 10?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will the classic CodeWarrior IDE work under windows 10?

1,503件の閲覧回数
fredstrathmann
Contributor I

I have an application written for the MCF52259 ColdFire processor.  I want to see if it will build under CodeWarrior.  I downloaded the classic IDE and attempted to install under Windows 10 on a 64-bit machine.  I get an error message that it will only run under 32-bit.  What are my options? (Thanks!)

タグ(1)
0 件の賞賛
返信
1 返信

1,381件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Google is your friend: https://community.nxp.com/thread/302974  :-)

0 件の賞賛
返信