Why did I fail with the following message when debug the.mcp project using MultiLink in CW v5.0\6.2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why did I fail with the following message when debug the.mcp project using MultiLink in CW v5.0\6.2?

1,499 Views
smecolive
Contributor I

When I debugged the.mcp project using MultiLink Universal and Code Warrior V5.0 and V6.2, I got an error after clicking the Connect(RESET) button and the following firmware upgrade failure message. In fact, I have already used PEFirmwareConfig.exe to update the firmware of MultiLink Universal from ARM to S12 type (because my target chip is MC9S12XEP100 and it use S12 architecture), I don't understand why the firmware is required to be upgraded again in Code Warrior IDE and cannot be debugable if the upgrade fails. The following is the corresponding picture, I hope someone can help me, thank you.

First update Firmware:

smecolive_4-1680759947103.png

Second :try to Debug

smecolive_1-1680759831327.png

Click no:

smecolive_6-1680760013487.png

smecolive_7-1680760033152.pngsmecolive_8-1680760051573.png

 

0 Kudos
Reply
1 Reply

1,493 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI smecolive 

Is this the same question as below thread?

https://community.nxp.com/t5/CodeWarrior-for-MCU/Failed-with-the-following-message-when-debug-the-mc...

If yes, please refer my reply there.

Thanks,

Jun Zhang

0 Kudos
Reply