Which IDE supports MM912G634 programming?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which IDE supports MM912G634 programming?

1,271件の閲覧回数
ralph_oberle
Contributor II

Hi all,

I try to figure out which IDE supports programming the above mentioned chip. It is a S12 based relay driver with LIN interface. But i could not find which S12 derivate I should choose in CodeWarrior to get the correct controller.

Greetings

Ralph

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,170件の閲覧回数
ralph_oberle
Contributor II

IDE:
CodeWarrior v5.1 eval --> 32kB Code Size maximum

Patch:
CodeWarrior for HCS12 v5.1 MM912 x634 ServicePack.exe

This should work ...

0 件の賞賛
返信