Which IDE supports MM912G634 programming?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which IDE supports MM912G634 programming?

1,268 Views
ralph_oberle
Contributor II

Hi all,

I try to figure out which IDE supports programming the above mentioned chip. It is a S12 based relay driver with LIN interface. But i could not find which S12 derivate I should choose in CodeWarrior to get the correct controller.

Greetings

Ralph

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,167 Views
ralph_oberle
Contributor II

IDE:
CodeWarrior v5.1 eval --> 32kB Code Size maximum

Patch:
CodeWarrior for HCS12 v5.1 MM912 x634 ServicePack.exe

This should work ...

0 Kudos
Reply