Where is CodeWarrior for HCS12 v5.1 MM912 x634 ServicePack.exe to download it

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is CodeWarrior for HCS12 v5.1 MM912 x634 ServicePack.exe to download it

ソリューションへジャンプ
2,810件の閲覧回数
javiervicandi
Contributor II

Hi,

We want to evaluate the adaptation of a product, MM912F634 based, to MM912G634. Our IDE 5.1 does not support the S12I64, inside the G634, and I guess we need this service pack. What rework would be necessary?

Thanks

Javier

0 件の賞賛
返信
1 解決策
2,664件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Javier Vicandi ,

 Yes, please download the service pack at here :

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=5901341    

(If this link can't open , you can also refer to the path below find it .)  

pastedImage_3.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,665件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Javier Vicandi ,

 Yes, please download the service pack at here :

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=5901341    

(If this link can't open , you can also refer to the path below find it .)  

pastedImage_3.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,663件の閲覧回数
javiervicandi
Contributor II

Thanks Alice Yang,

Something about possible changes for adaptation?

Best Regards

0 件の賞賛
返信