Update to FreeMASTER 2.0.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Update to FreeMASTER 2.0.2

2,293件の閲覧回数
jtpark
Contributor IV
Hello,
I used 2.0 version of FreeMASTER.
However, after I updated to 2.0.2, I cannot input decimal and odd number to real type transformation of Variable tab.
Would you help for this?
Thanks.

Original Attachment has been moved to: SCR-Cooling-20W-EWP-내구시험.pmp.zip

Original Attachment has been moved to: S12ZVML-MINIBRD_BLDC_Sensorless_CW_IDE.elf.zip

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,951件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

- For solve your problem , could you please provide more information :

1. how to reproduce your problem?

2. problem screenshot.

- Dose change this place can help you ?

pastedImage_1.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,951件の閲覧回数
jtpark
Contributor IV

Dear Alice,

Please see the below.

1. how to reproduce your problem?

--> I removed the FreeMASTER ver 2.0.0 using uninstall file. Then I installed the FreeMASTER ver 2.0.2.

After finish installing 2.0.2, start the '.pmp' file made of ver 2.0.0. Then, entered the value at the Variable Watch. I can enter the odd number and decimal(ex, 11, 11.1) in ver 2.0.0 but ver 2.0.2 can't.

I saw the similar question with my problem in NXP homepage and applied that manner. First, I made the new '.elf' file through build and debug in codewarrior. Then applied to new '.elf' file in FreeMASTER ver 2.0.2 but wasn't change anything.

 

2. problem screenshot.

-->Please attached file.

 

- Dose change this place can help you ?

-->I don't understand what you are saying. Please the explain more detail.

Thanks.

2_0_0.JPG2_0_2(1).JPG2_0_2(2).JPGuninstall.png

0 件の賞賛
返信

1,951件の閲覧回数
jtpark
Contributor IV

Dear Alice,

I added your answer.

- Dose change this place can help you ?

-->Please see the below.

    I use the real type transformation. So, I can't change the other type.

variable.JPG

Thanks.

0 件の賞賛
返信

1,951件の閲覧回数
agostinofacotti
Contributor III

Hi J.T. Park,

I've the same problem as yours with Freemaster 2.0.2 (see https://community.nxp.com/thread/435986 ) but using linear interpolation instead of two point: in my case Freemaster accepts only values that transformed-back gives an integer number.

Best regards,

agostino

0 件の賞賛
返信